STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! Issue Building CM0Plus project

Hello,Context: New to stm and HAL. Creating a new dual-core STM32 project on a NUCLEO-WL55JC1 board. Starting from cubeMX generated code with basically only RTC initialized on Core M4. Using STM32CubeWL Firmware package v1.3.1 . M4 builds and loads g...

lame_stmr by Associate III
  • 2013 Views
  • 4 replies
  • 1 kudos

Nucleo-WB05KZ power consumption

Hello I have a nucleo wb05kz programmed with BLE_Power_Consumption example project (STM32Cube_FW_WB0_V1.1.0 package) and i want to measure the current consumption.Following the UM3343, I removed the JP1 and JP2 jumpers and connected my power supply (...

Resolved! STM32WL55 and STM32WLE5 HW compatibility

Hi,I would like to confirm that STM32WL55 and STM32WLE5 are mutually HW compatible from the point of external circuitry? I.e. can we use either one in a PCB originaly designed for one of them w/o any modifications? (Yes, I checked both datasheets but...

MMici.1 by Associate III
  • 785 Views
  • 1 replies
  • 0 kudos