cancel
Showing results for 
Search instead for 
Did you mean: 

Need suggestion for LORA module compatible with I-CUBE-LRWAN

YGagn.1
Associate

Hi.

Can someone confirm that the I-CUBE-LRWAN software supports any SX1262 or SX1276 modules? That's what I understood from reading the details of the software package.

I'm looking to create a custom PCB with a STM32L4 mcu and I was wondering if anyone could recommend an SX1262/1276 module.

Thanks

2 REPLIES 2

Well historically yes,but most "modules" these days come with an MCU

As I recollect I had to port onto the L4 platform

Perhaps look a Seeed, Reyax and Heltec, and ST's STM32WL series

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

It depends on what you mean by, "support".

ie, whether you're prepared to dig into the low-level SX12xx chip stuff, or if you want something that will "just work" out-of-the-box ...

https://www.st.com/en/embedded-software/i-cube-lrwan.html

 

PS:

At the SX12xx chip level, the  I-CUBE-LRWAN code is just Semtech's anyhow.

Try Semtech for MCU-agnostic code...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.