NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Posted on June 29, 2017 at 18:12Hello,We've got two B-L072Z-LRWAN1 LoRa Discovery kit boards and we're trying to use the end_node demo project, included in the https://my.st.com/content/my_st_com/en/products/embedded-software/mcus-embedded-software/...
Posted on June 29, 2017 at 14:30Hi Support TeamI want to implement sleep mode in ping pong project , so slave device send some data and go to sleep ..STM32L072CZYX - LORA DISCOVERY boardhow to put the device into sleep mode , please share some docu...
Posted on June 27, 2017 at 11:02Hi Support TeamQuestion 1 :I am using ping pong in ST-LORA discovery kit .I used cubeMx to generate code for reading i2c temprature/humidity sensor , it is working , here /** System Clock Configuration*/void SystemClo...
Posted on June 13, 2017 at 11:05Hello folks,it seems like there is a very important topic not discussed right now. There are LoRa examples for System Workbench for 5 different Boards, which include in the folder middleware all functions of LoRaWAN. ...
Posted on June 13, 2017 at 00:16I was doing a firmware update over the air and it failed, so now I don't have the LED blinking on my SensorTile. How do I recover from this? Also, could it have been because the SensorTile was not blinking constantly ...
Posted on May 24, 2017 at 11:04Here the procedure : - Join -> Join OK - Uplink , a downlink is send by the networkat this point sometimes (near 25%), no more uplink is send after.I did not success to reproduce this problem in debug mode to understan...
Posted on April 24, 2017 at 14:43A lots of time, the timer used to switch off the TCXO of the LoRa Module seems to block the timer utility. As this one stay indefinitely on the head.Did someone see already this problem ?#i-cube-lrwan
Posted on April 25, 2017 at 13:11Hi,I bought two STM32 Nucleo-L073RZ pack boards with expansion LoRa boards. I downloaded from STM32 site the example projects for board and I tried to run project for LoRa called PingPong. This project should start t...
Posted on April 10, 2017 at 20:50Hello everyone, I am using STM32F070RB with SIM808 on board. I just want to have FOTA feature in my design so that program can be updated remotely via GPRS. The current program size is of 67KB (i.e., 61KB internal pr...
Posted on April 04, 2017 at 11:41I am using I-CUBE-LRWAN firware.But have different controller STM32L082 instead of STM32L053 mentioned in End node example Application.By default it have OTAA,I changed to ABP method.I am using SX1276 radio and i hav...