STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

B-L072Z-LRWAN1: improving the reach

Posted on November 16, 2017 at 23:52I purchased three B-L072Z-LRWAN1 nodes yesterday and started my long awaited experimenting. The distance while maintaining stable communication between two B-L072Z-LRWAN1 nodes is a bit of a dissapointment. After ...

USI WM-SG-SM-42 point to point communiation

Posted on November 03, 2017 at 15:02Hello,Using 2 WM-SG-SM-42 modules which are parts of I-NUCLEO-LRWAN1 I am trying to establish point to point communication without LoRaWAN. I have updated the AT commands firmware to 3.0 and I am following the exa...

maciek by Associate II
  • 2448 Views
  • 7 replies
  • 0 kudos

P-NUCLEO-LRWAN1 CAD function

Posted on October 25, 2017 at 15:37I'm developing application with P-NUCLEO-LRWAN1 modifying I-CUBE-LRWAN software.But i could not trigger CAD (Channel Activity Detection) function. And i'm not sure that interrupt for CAD_DONE (DIO3) is enabled or n...

Chris Oh by Associate II
  • 1024 Views
  • 1 replies
  • 0 kudos

Resolved! LoRaWAN with MultiTech Conduit Gateway

Posted on October 20, 2017 at 19:16I have: B-L072Z-LRWAN1 Discovery board (based on muRata module)P-NUCLEO-LRWAN1 Pack (Nucleo-64 board with Semtech SX1272 bare chip add-on).I-CUBE-LRWAN firmware pack, v1.1.2Keil MDK for STM32L0/F0, v5.24aMultiTech...

0690X00000608jSQAQ.png 0690X00000608WgQAI.png

OTA Update

Posted on September 26, 2017 at 08:34Hi Dear, We want Low Power With OTA update based  Micro-Controller Please Suggest me Which are the Best Solution. Thanks!Nitin Kanani #ota #stm32f