NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello,I am very very new with STM32 and I am doing a challenge. I am working on a Macbook AirI have at my disposal aThe B-L072Z-LRWAN1 Discovery kit A st-linkA j-linkMy goal is to build a Gateway-repeater with BL072Z-LRWAN decovery kit, with the fo...
I have installed the recent version of CubeMX - 5.2.1.I have downloaded STM32CubeExpansion_LRWAN_V1.2.1.When I try to add it in the Embedded software package manager, I get a message: This package version is not managed in the version of STM32CubeMX.
Hello !I'm sending a LoRaWAN message tothe ping pong code wich plays the role of a gateway but the message is received encrypted , I need to decrpt it on the reception side.Any help please thank you!
Are there any documents that describe the use of the scheduler or the openThread API in more detail? A little more detailed explanations of using the openThread api and the Scheduler would be very useful.What are the advantages of using this Schedule...
The murata Lora module CMWX1ZZABZ is used and the STM32L072 is inside.Can the STM32 internally reset itself without using the reset function?Explain what happens if a reset occurs.
I am getting invalid values for the device id and package data from the STM32WB55 on a P-NUCLEO-WB55 Nucleo board.I am getting a value of 0x26 for the Device ID in the UID64 at 0x1FFF7584. And I am getting a value of 0x13 for the package type in the...
Hi,I have some experience with BLE and Nordic devices (mostly nRF51822 and BLE 4.1).The Nordic provides sniffer firmware for their devices and I used it a lot. ---Now, thanks to ST team, I have the P-NUCLEO-WB55 kit in my hands and started playing wi...
Binary Install Address for STM32WB5xxE(512K) and STM32WB5xxC(256K) devices.Hi!In Release Note for STM32WB Copro Wireless Binaries writes what is install address for stm32wb5x_FUS_fw.bin depending on the chip model, as:STM32WB5xxC(256K) - 0x0803E000ST...
error:.\mlm32l07x01\NUCLEO_CUBE_LORA.axf: error: L6050U: The code size of this image (52352 bytes) exceeds the maximum allowed for this version of the linker.Finished: 0 information, 0 warning, 0 error and 1 fatal error messages.".\mlm32l07x01\NUCLEO...