STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 235 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4077 Views
  • 0 replies
  • 3 kudos

ATT_MTU size

HI,Does someone can explain me how to modify the ATT MTU size please ?Thanks.

LVent by Associate II
  • 3842 Views
  • 5 replies
  • 0 kudos

How to create a private service in the firmware?

There is a heart rate service example in the STM32WB firmware. If I want to create a private service in the firmware. For example​, I want to create a service to let the LED on and OFF. How to create a private service like that?

Rzou by Associate
  • 623 Views
  • 0 replies
  • 0 kudos

Resolved! Modify Ping-Pong example

Hi guys,I program an application with a STM32LO-LRWAN1 module who does the connection with a sensor by I2C and i would like to integer my application in the "Ping Pong" example for proving to my boss that the connection between two modules is possibl...

mibou23 by Associate II
  • 2919 Views
  • 4 replies
  • 0 kudos

Resolved! Iam unable to debug STM32 B-L0722Z-LRWAN1 board having onboard STM32L072CZ MCU. It gets programmed but no respose for breakpoints and also unable to suspend

Attaching the log files.Open On-Chip Debugger 0.10.0+dev-00021-g524e8c8 (2019-04-23-20:37)Licensed under GNU GPL v2For bug reports, read http://openocd.org/doc/doxygen/bugs.htmlsrst_only separate srst_nogate srst_open_drain connect_assert_srstInfo : ...

Resolved! where can I download the AN5289

I want to build the wireless application. I see the an5289 is a guide for that. but I can't find where I can download it.

cchao by Associate II
  • 1848 Views
  • 5 replies
  • 2 kudos

ping pong with lora doesn't recieve anything working on theboard B-l072Z-LRWAN1 with I-CUBE-LRWAN firmware packag?

I'm working with the ping pong with lora in stm32 , the code doesn't recieve anything , it only executes the RX_timeout and TX_timeout while the device in the other side is sending DATA correctly with lora, How can I fix this problem ?this is in the ...

AChaa.15 by Associate II
  • 999 Views
  • 1 replies
  • 0 kudos