STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 220 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

stm32wb55 with STM32CubeIDE

I've been following the stm32wb workshop using the stm32cubeIDE and i been running in to some difficulties, due to all the documentation being out of date and also unable to run any of the examples on the cubeIDE, has anybody managed to create a proj...

Increase size of sent data by BLE client

Hi! I flashed my USB dongle with BLE_p2p_client application that I edited on my own. But I can not send more than 3 bytes using aci_gatt_write_without_resp in function tBleStatus Write_Char in the file p2p_client_app.c . Even if I increase CharValLen...

Kolab by Senior
  • 1111 Views
  • 3 replies
  • 0 kudos

What are limitation of Different BLE network topology ?

Hi,As we are at the very beginning level of project, and exploring different BLE network topology.1st i would give an overview of the system that we are planning to implement.We have BLE devices / sensors (Appox 100 nos) which are fitted in small com...

RSakh.1 by Associate II
  • 605 Views
  • 0 replies
  • 0 kudos

Resolved! Cannot send more than 1 byte!

I'm using two STM32L4xx connected to LoRa modules. The LoRa settings on both cases are:bw = 500 kHzSF = 12CR = 4/5implicit header, Crc off, low data rate optimization is on.On transmitter module, I do the following:Make sure the module is not in slee...

MHoss.1 by Associate III
  • 1496 Views
  • 1 replies
  • 0 kudos

STM32WB55 does not advertise

Hello! I welded the controller p-nucleo-wb55 on my board(out of debug board) and powered it how is described in the documentations, but bluetooth does not work(does not advertise). How can I solve this problem?

Kolab by Senior
  • 926 Views
  • 2 replies
  • 0 kudos

When I increase the spreading factor on my CMWX1ZZABZ, which uses a STM32L and SX1276, I keep getting a OnTxTimeout.

If the spreading factor is set to 9, messages get through. As I increase it to 10 or 11, I start to get the OnTxTimeout error. The payload I'm sending is similar to this lCrTHfXrQdM7M6ZoFrmwMxHacVtZcoBxvSvve0Pi5awSYtk=I need to increase the spreading...

GStew by Associate
  • 1070 Views
  • 1 replies
  • 0 kudos