Has anyone been successful connecting the BlueNRG-2 SKD (IDB009V1) to either the BlueNRG ST-LINK UTLITIY or IAR 8.40? Both utilizes "CAN'T DETECT". The only tool that seems to detect the SDK is the cumbersome Flash Programmer.
have a default location X. If want to update the code, i download it to location Y and expect the STM32 to start at location Y after reboot. However, the routine keeps rebooting from X. what am i missing?