2020-04-29 12:10 PM
If the spreading factor is set to 9, messages get through. As I increase it to 10 or 11, I start to get the OnTxTimeout error. The payload I'm sending is similar to this
lCrTHfXrQdM7M6ZoFrmwMxHacVtZcoBxvSvve0Pi5awSYtk=I need to increase the spreading factor to increase the range. My frequency is set to 904600000 and my bandwidth is set to 2.
2020-04-29 1:04 PM
You'll need to expand the timeout to accommodate the amount of time it takes to send the message.
Perhaps use Semtech's LoRa Calculator to understand the timing/constraints.