STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 240 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4082 Views
  • 0 replies
  • 3 kudos

STM32WLE5JC disabling context management

We have developed an IoT sensor using the STM32WLE5JC LoRa module. It is a device we expect to reboot a few times (when necessary).  It was discovered that when a downlink command (to reboot the device) is sent, the device reboot, but then it hangs d...

Resolved! I cant login https://my.st.com/sfxp

I'm developing a Sigfox product using the STM32wlxx series.For testing purposes, I'm trying to provision Sigfox using the STM32 programmer,but I can't log in using the link https://my.st.com/cas/login?service=https://my.st.com/sfxp.

login_error.png
HongKwon by Associate
  • 421 Views
  • 1 replies
  • 0 kudos

Help with custom bootloader for STM32WL5MOCH6TR

Hello,I wrote a custom bootloader (that loads firmware image from an external flash) for a device that was using an STM32WL55CCU6. Now I want to use the same bootloader on a device with a similar uC, the STM32WL5MOCH6TR.The bootloader works correctly...

STM32WB5MMG - LCD module abnormal consumption

Hi everyone, I'm experiencing abnormal power consumption in STOP2 mode with my custom board featuring the STM32WB5MMGH module. According to the datasheet, the power consumption in STOP2 mode should be between 2 and 3 µA. However, my board is drawing ...

CSharpino by Associate III
  • 904 Views
  • 1 replies
  • 0 kudos

Resolved! NUCLEO-WBA55CG Transparente Mode Example

Hello Together,I would like to try out the STM32CubeMonitor-RF (V2.15.0) with the NUCLEO-WBA55CG board. I downloaded the stm32cubewba mcu package (V1.7.0) and flashed the .bin file from the BLE_TransparentMode example to the board with the STMCubePro...

Resolved! Cable replacement feature on Android

We need some help with cable replacement feature. Our project using WB1M as a client device, sharing data over UART. Android application must be server. STBLESensor_Android source code not include any sample code with Cable replacement feature. Were ...