cancel
Showing results for 
Search instead for 
Did you mean: 

Accepting / rejecting pairing requests on STM32WB55

tmk
Associate II

Hello, 

I am using STM32WB55 chip on my custom setup. I have configured my device in peripheral mode. I want to be able to accept / reject pairing requests initiated by the client device. I am following AN5270 for development. I have added code to set bit3 in SMP_MODE register to enable the generation of pairing request event. Although, the documentation says "SMP MAY generate the event". Why is that? 

tmk_0-1741228230220.png

The documentation also says that if I bypass the SMP, all the events that go to SMP will be transmitted to the application. However, what are the other events handled by SMP? I am not able to find a list of events handled by SMP. Is there any other documentation that I am missing? 

I also looked at an older thread in which the functionality to accept / reject pairing request did not exist. But since not it exists, do you have an example code where it actually works?

Any help is appreciated!  Here's the old thread: https://community.st.com/t5/stm32-mcus-wireless/what-is-the-api-call-to-get-the-stm32wb-to-reject-all-pairing/td-p/89769

1 ACCEPTED SOLUTION

Accepted Solutions
tmk
Associate II

I resolved the issue. Turns out I was using a very old firmware version for Bluetooth. Updating to latest firmware solved the issue immediately. 

View solution in original post

1 REPLY 1
tmk
Associate II

I resolved the issue. Turns out I was using a very old firmware version for Bluetooth. Updating to latest firmware solved the issue immediately.