User Activity

We use STM32L162xx MCU to communicate with S2_LP and SP_BTLE drivers via SPI. With S2-LP, it returns the MC_STATE as READY during inital setup for power , sync word etc.But when I Strobe the RX command it returns MC_STATE as LOCK_ST(0x14). DMA is ena...
The device is designed i  a way that, it should wake up every 30 seconds via RTC wake up timer or upon button press, read sensor values (for temperature and humidity ), if there is any change in these values , send packets via radio (SUBGhz) and ente...