NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I'd like to validate that a given wireless firmware image will install before attempting to erase the existing wireless firmware stack (we have external storage via SPI that we download updates into). Since the firmware images are signed so that the...
Hi I am trying to use the AT-Slave application from icube lrwan stack on b-l072z lrwan in the IN865 band. When I give AT comand, I get AT_ERROR as response. Please help.Thanks,Mary
Is there a difference in hardware for these communication protocolls? Or is it possibile, that there will be sometime a wifi stack for the STM32WB?
Hi, recently I made a custom board with STM32WB55RGV6 but my BLE side isn't working.I used STLink to flash in the CoPro lib FW as shown in the YouTube link below.https://www.youtube.com/watch?v=AcrbUOhApd0I used the P2P_Server example for Nucleo boar...
I'm trying to make all of my STM32WB55 Zigbee network run on batteries. The SEDs are easier enough, but I need a solution for the coordinator. My current plan is to disable the Zigbee radio when not in use. What is the process to disable the Zigb...
I am a beginner with STM32 and the NUCLEO-STM32WB55 board.The preflashed demo application worked without problems. When I installed the STM32WB55 MCU package, a couple of examples were available like the BLE HRS service.I managed to import the projec...
Hello,I am trying to use the STM32WB55 Nucleo Pack to develop a BLE application. I am using cubeMX with the STM32Cube_FW_WB_V1.8.0 pack to generate code for the MB13355C nucleo board with STM32WB55RGV6 MCU.I have successfully set the BLE advertising ...
I was wondering if it would be possible to know if adafruit’s VC0607 camera with the P-Nucleo-Wb55 board.i’m not receiving any data back from the camera and i saw that there’s other stm32 that handles jpeg multimedia that this P-Nucleo doesn’t
Hello, i'm trying to sense the temperature via ADC (DMA) and then pass it to the wireless-core M0 in order to show it on my smartphone, e.g. by using the already existing body temperature profile in the STM BLE-applications. In this existing applicat...
Lora class c unconfirm message uplink return LORAMAC_STATUS_NO_FREE_CHANNEL_FOUNDI had downloaded en.I-CUBE_LRWAN. I am using Projects -> B-L072Z-LRWAN1 - > MDK ARM.I am using Class C. I had try change the APP_TX_DUTYCYCLE and it does not help.#defin...