STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

CLASS C NOT SENDING ANY PACKET. I-CUBE-LRWAN 1.3.1. Class C

Hello,Can someone help me?I work with STM32CubeIDE, I-CUBE-LRWAN, Import End_Node Project example, config everything to work on Class C.Device successfully join to the network, and switch to class C done appears on Serial terminal. But, when the upli...

0693W0000059IT4QAM.png
fery_rz by Associate
  • 1156 Views
  • 1 replies
  • 0 kudos

WB55 CoPo IAP-programming: system-table missing

I need to be able to install/upgrade the CoPro from CPU1.I get the FW for CPU1 and CPU2 by its system-bootloader via SPI from another STM32-MCU. Sadly FUS-commands in the System-bootloader are only supported by USB and UART. Studying AN5185, this tas...

0693W000005AFsIQAW.jpg
CHr by Associate
  • 810 Views
  • 0 replies
  • 1 kudos

Resolved! unknown type name '__RAM_FUNC'; did you mean '__ARM_FP'?

I trying to port STM32CubeExpansion_LRWAN_V1.3.1 for the evaluation board B-L475E-IOT01A2. I managed to whittle the errors down to 2. In both cases i am getting unknown type name '__RAM_FUNC'; did you mean '__ARM_FP'?in a HAL file stm32l4xx_hal_flash...

DNeet.1 by Associate II
  • 4385 Views
  • 3 replies
  • 0 kudos

Really basic question about HAL_USART_RxCpltCallback function

Hello everyone!I'm trying to setup a very basic application and currently have my LPUART Tx and Rx pins tied together. I'm able to run the following code without any issues (well, this is the core of the code with all the initializations stripped out...

JBee.1 by Associate II
  • 3070 Views
  • 4 replies
  • 0 kudos