Dear all,I am trying to set-up the internal PLL for running @ 48-MHz.I can easily set-up the clock tree to achieve frequencies lower than 44-MHz, but when I try 48-MHz, the cpu does not end from the loop that verify that the PLL is OK.The FLASH is se...