NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello. What is the value of the internal reference voltage of STM32WB55RGV6 MCU?Is it 1,212 V or 2,048 / 2,5 V?
Hello. What is the exact value of T_coeff_vrefint? I'm planning to use internal reference voltage buffer (VREFBUF) output pin in my application.
Stm32wb BLE callback function: void hci_disconnection_complete_event( uint8_t Status, uint16_t Connection_Handle, uint8_t Reason ){ printf("hci_disconnection_complete_event");}not working.STM32WB use a utility f...
I am working on a project using the STM32WB55xx series. I'm trying to read the Device Information Table (AN5185 Section 6.6.1, pg 17) using a bash script and the STM32 Programmer CLI.According to the documentation (AN5185 Section 1.2 page 3) I should...
Hello,We are working on integrating Wi-Fi module Murata Type1 MW LBEE5HY1MW(Cypress CYW43455) with STM32F4 based micro-controller using SDIO interface.We are looking for SDIO Driver and Murata Wi-Fi driver for STM32F4 based micro-controller.anyone he...
The ERRATA says essentially that port activity on PA2/PC13 will disturb LSE (WCLSP100)Does that mean that I can use PA2 still as LSCO ?Does that also mean that I still can use PC13 as RTC_TS / RTC_TAMP, or as WKUP2 ?Which ones will be a problem, or i...
Hi, Can anyone please explain the difference between Radio.StartCad and Radio.SetRxDutyCycle in LoRa?I am clear with the SetRxDutyCycle function but not sure what is the difference between CAD and duty cycle?
Hi, I am developing a sigfox app using stm32WLE5JC. I am reading it using cube programmer and on sigfox tab the chip certificate reads all FFFFFFFFFF . I also tried to read the sigfox PAC and ID on the 0x0803 E500 but its al FFFF. I want to ask how c...
Hello,today I just ran the heart rate demo and suddenly the board seems to be bricked. The onboard debugger is running, but the CubeIDE is unable to start a GDB server. Using the ST-LINK utility I wasn't able to establish any connection to chip. So i...
Hi,I want to build a simple point-to-point communication (2 devices for now) system between two NUCLEO-55WLJC1 dev kit.I would like to use the LoRa modulation for this purpose but do not want to use the complete LoRaWAN protocol (and its stack).Is th...