STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

I-CUBE-LRWAN, questions..

I am using I-CUBE-LRWAN to create a LORA end-node device. But the documentation does not say anything about how to create your own device using this extension. I have two questions:1) Can this extension be integrated into CubeMX?2) Are there instruct...

mak1308 by Associate III
  • 1088 Views
  • 1 replies
  • 0 kudos

stm32wb5mm-dk ble freertos project

hi,I need to run a freertos ble project on stm32wb5mm-dk board like "BLE_HeartRateFreeRTOS" example project avaiable for p-nucleo-wb55 board, but there isn't any avaiable and if I try to replicate it from new project it don't work, "APP_BLE_Init()" i...

LBera.1 by Associate II
  • 1473 Views
  • 2 replies
  • 0 kudos

How to use USART1 to send/receive data packets (for serial application) and LPUART1 as Virtual COM Port in STM32WB5MMG-DK?

Hi,I am using STVM32WB5MMG-DK for my project development activities.When I referred the user manual "UM2825", I came to know that the STM32WB5MMG USART1 interface is connected to the UART2 port of the STM32F103 ST-LINK/ V2-1 MCU.Is there anyway that ...

PB S.1 by Associate II
  • 2103 Views
  • 1 replies
  • 0 kudos

How to reset the P-Nucleo-WB55 to original and what are the possible problems with the sample code (BLE_HeartRate)?

I am new to this area and I just bought two P-nucleo-wb55 boards. When I used the p2p server example, it can work properly and I am able to use my phone to control the on/off of the led. However, when I tried with another sample 'BLE_HeartRate', it c...

MX.1 by Associate II
  • 1909 Views
  • 3 replies
  • 0 kudos

How to provision LoRa devices?

STM32WL55 family devices need unique credentials on a chip-by-chip basis. These include DevEUI, AppKey and AppEUI, as well as Region etc.What strategies are there to permit this provisioning during the manufacturing process?I am thinking of this proc...

charles23 by Associate III
  • 2495 Views
  • 2 replies
  • 0 kudos

STM32Wl getting sent Data with OnRxDone

Hello there!I just modified the PingPong example for the NUCLEO WL55JC1 Board so I have one defined transmitter and one receiver.As you can see in the picture, the Master transmits continuously the bytes "PING" (wich I want to replace later). /* Send...

GHube.1 by Associate II
  • 1580 Views
  • 2 replies
  • 1 kudos