STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

STM32WL with HSE and XTAL

I am trying to start HSE with external crystal (on nucleo WL55JC1 board). I removed R2 (Output from TCXO), added two 0E bridges R39 and R40, added 10k resistor R41 (to remove stub). Then I started the Cube-MX (latest, fresh update...), selected the n...

0693W00000D15ucQAB.jpg
s54mtb by Associate II
  • 3212 Views
  • 3 replies
  • 0 kudos

Is it multi-regional application possible?

Hi, everyone. Is it possible to build an application that supports all regional standards? AS923-1 / AS923-2 / AS923-3 together are of particular interest (depending on the setting, which is changed via the UART, for example).

OSole.1 by Associate II
  • 1330 Views
  • 2 replies
  • 0 kudos

Fram write/read error, with stm3wb55?

Good afternoon to all forum members. I have a problem with stm32wb55 and i2c protocol. I use i2c (hi2c3) with the connected peripherals Ad7746, adxl345, mcp9808 and they work fine, but if I join fram MB85RC256v, with the write/read in the routine I w...

A Bravos by Associate III
  • 1871 Views
  • 2 replies
  • 0 kudos

WL55CC print_f io redirect UART busy

I am trying to setup UART1 on WL55CC; using RTS; #include <stdio.h>   #if defined (__ICCARM__) || defined (__ARMCC_VERSION) #define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f) #elif defined(__GNUC__) /* With GCC, small printf (option LD Linker->L...

bblouin by Associate III
  • 733 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE project based on end_node example

Hi,I have already got the example end_node running, however, i now want to start a new project based on this example. I would like to have all Drivers and Middlewares inside the project and not just links to those files. I had many attempts trying to...

KKull.1 by Associate
  • 1796 Views
  • 5 replies
  • 0 kudos

How to implement a a BLE, with a sensor in the MCU STM32WB55

Hello to the forum. I would like to start working with stm32wb55, due to its low consumption and also because it has the BLE protocol. However, I cannot find how to implement and link the cpus. I ask if anyone knows where I can get simple and practic...

A Bravos by Associate III
  • 1241 Views
  • 2 replies
  • 0 kudos