NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Programmed OB IPCCDBA to 0x800Value of OB struct.ipcc data buffer:Name : OptionsBytesStruct.IPCCdataBufAddr Details:536903680 Default:536903680 Decimal:536903680 Hex:0x20008000 Binary:100000000000001000000000000000 Octal:04000100000Value of pMb_RefTa...
The ZbNwkIfSetTxPower func is set tx power,but i don't know this function's parameter NAME(interface name) ,how can get this value?
Hi, we are going to use two PSRAM devices to STM32's QuadSPI interface. Each PSRAM device has its own chip select line cs_b. How do we have such control with the _NCS line in a single-bank quadspi interface? Should we use two extra lines of GPIO sepa...
hi,I'm trying to create a freertos based ble poject on stm32wb5mm-dk board like ble_heartrateFreertos example avaiable for p-nucleo-wb55 board. I have changed sys time base to tim17 and enabled freertos and stm_wpan, and in clock configuration I have...
Hi,I'm working on a BLE app using an STM32L4 as main processor and a BLuenrg-m2sa as network coprocesor for the BLE stack. have develop the app code and setup all the gatt services and characteristics. Also developed an android app to connect as cent...
I've setup a P2PServer based firmware created from CubeMx. So far so good. It advertises as expected. But when I run the lightblue app, it won't connect to my advertising device.I've already compared my firmware to the P2PSERVCE example project from ...
I'm working on both custom board and P-NUCLEO-WB55. Trying to reach the lowest power consumption as possible I just detected that the measured current in STOP2 is around 50uA (BLE off and RTC ON) instead ~2uA. The result is comparable between boards,...
I'm looking for an example. Can you help me?
Please, exist some tutorial or an example how to use the list of allowed devices to connect? I know the allowed device addresses.