STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos
Rvan .8 by Associate II
  • 1222 Views
  • 1 replies
  • 0 kudos

Resolved! Problems with GPIO.

I'm working with the NUCLEO-WL55jc1 board and I have one strange behavior. I need one output pin and I've called it Trigger.Initially, the pin PC2 was used but I wasn't able to make it work. It had incorrect output voltages and some bounce like it wa...

0693W00000DpxlKQAR.png
FRest.1 by Associate III
  • 2193 Views
  • 5 replies
  • 0 kudos

No STM32 Target Found - Custom board

Hi guys, I recently made a design based on nucleo wb55 dongle using STM32WB55CGU (48-UFQFN), but I cannot connect to it using SWD. I believe it is not a schematic problem, so I am a bit stuck for debugging the situation. I soldered it using hot air s...

0693W00000Dq0DGQAZ.png 0693W00000Dq0TsQAJ.png 0693W00000Dq0D6QAJ.png 0693W00000Dq0D1QAJ.png
TEsli.1 by Associate II
  • 3301 Views
  • 13 replies
  • 0 kudos

Example QSPI_ReadWrite_DMA does not work on STM32WB5MMG board

I am working on STM32WB5MMG board and using the example QSPI_ReadWrite_DMA.In the main function the program can not run into case 2 to call HAL_QSPI_Transmit_DMASource Code as below:   case 2:    if(StatusMatch != 0)    {     StatusMatch = 0;     TxC...

ALai.2 by Associate II
  • 2336 Views
  • 4 replies
  • 0 kudos

stm32wb5mm-dk custom service and characteristics

Hi, In my application I have added a custom service with 5 characteristics, all have 128bit UUID, 3 characteristics are 4 byte long and 2 characteristics are 2 byte long.When I compile and connect to board by my phone I can't see the last charactersi...

LBera.1 by Associate II
  • 941 Views
  • 0 replies
  • 0 kudos

how to maximize STM32WB BLE throughput

Hello friends,I am working on STM32WB on-chip Bluetooth low energy system to transmit data from server to client using notification property.I want to transmit 46 bytes at the rate of 500Hz without any packet loss, to achieve this I have updated the ...

Aishwarya by Associate III
  • 1822 Views
  • 0 replies
  • 0 kudos

ZigBee OTA

Hi,is there anyone who tries to run ota zigbee example? After some debug I think that ota client is unable to write data to flash.From the server side I can see that the process started. From the client side I can see the red led on what mean abort d...

lukasz2 by Associate III
  • 1801 Views
  • 2 replies
  • 0 kudos

STM32WB55 USBDongle ERROR (Zigbee FFD & Application example)

Hi there, I'm struggling with the P-NUCLEO-WB55 kit I just bought...! I wanted to try basic application example given in STM32WB package, followed the documentation and nothing works correctly on the USB dongle...!Application : Zigbee_OnOff_Client_Ro...

DPerr.2 by Associate
  • 1288 Views
  • 1 replies
  • 0 kudos