STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

I-CUBE-LRWAN AT_SLAVE example AT_DevEUI_set

HelloI am experiencing two problems.My development environment is STM32L072CZ-LRWAN1.You are now using a combination of END_NODE and AT_SLAVE examples.I'll sort out my problems.The first is that 'SET' values are not operated through features such as ...

0693W00000D1475QAB.jpg 0693W00000D147UQAR.jpg
SYun.2 by Associate III
  • 1122 Views
  • 1 replies
  • 0 kudos

Fail und FUS and Stack update

Hi everybody,I think I have the same problem as CTare (https://community.st.com/s/question/0D53W00000fo0kcSAA/unable-to-install-wireless-stack-on-stm32wb55?t=1628516513992) I coudn't reply to that post because it's already archived. My setup: Nucleo ...

mkrug by Associate III
  • 3107 Views
  • 9 replies
  • 0 kudos

Low Power on STM32WB without 32KHz Crystal

Greetings,From what I've read of the Cube code and guidance in AN5289, we enter STM32WB low power states by putting the M4 into the low power state we want. If we need the M0 to continue to advertise, for example, we would configure it to do so and ...

How to update Mesh Proxy Data Out?

Hello,I have mesh node with proxy feature. After provision, I can see that node advertising Mesh Proxy Service (UUID 0x1828), How can I update Mesh Proxy Data Out (UUID 0x2ade)? I spent a lot of time searching for some callback or function, where I c...

fiiita by Associate
  • 1117 Views
  • 1 replies
  • 0 kudos

API Sigfox without prototype (SIGFOX_API_send_frame) and dont works. (STM32WL Single Core versions 1.1.0 and 1.0.0)

The API (SIGFOX_API_send_frame) found in the examples of PushButton and AT_SLAVE of STM32WL SINGLE CORE (https://www.st.com/en/embedded-software/stm32cubewl.html), versions 1.1.0 and 1.0.0, is without prototype and the sigfox does not work (does not ...

MRebo.1 by Associate II
  • 5246 Views
  • 11 replies
  • 0 kudos