STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! How to use HAL_I2C with repeated start conditions

Hello! I'm trying to interface with a sensor that requires a repeated start condition.Datasheet: https://www.mouser.com/datasheet/2/348/ROHM_S_A0005047448_1-2562246.pdfI have other sensors on my I2C bus that I can communicate with. I also get '1' on ...

WSher.1 by Associate II
  • 3047 Views
  • 4 replies
  • 0 kudos

Disable UART on I_CUBE LRWAN

I have a custom board running the i cube lrwan (class A). I m going to deploy it in the field, so I dont want any messages coming on the UART. Is there a way to disable it ?When I add too many print statements for debugging, the LoRa Initialisations ...

BSada.1 by Associate
  • 1154 Views
  • 1 replies
  • 0 kudos

STM32WB55 SYSTICK AND RUN ISSUES

Hey thereI'm working with stm32wb with custom board, I have two strange issues.I'm tying to probe GPIO_IOToggle example but the program only run when i charge the code or when I debugged it with STM32CUBEIDE, whne i press reset or activate the source...

JGome.7 by Associate
  • 1459 Views
  • 1 replies
  • 1 kudos

How to make a LoRaWAN End Node with STM32WLE5J8I ?

Helloi made a custom board using MIDATRONICS module that integrate the STM32WLE5J8I and i don't find how to make a lorawan end node project !!! when i import the end node project from the nucleo-WL package, it doesn't work (don't make a join and don'...

SHATE.1 by Associate III
  • 2507 Views
  • 5 replies
  • 0 kudos

Write/Erase flash results in hard faults in BLE application

Dear ST communityI've been trying to implement the BLE_RfWithFlash example from the STM32WBCube package into my BLE application.When trying to write/erase flash, the MCU disconnects the BLE client and triggers a hard fault. If I run the application i...

KMeld.1 by Associate III
  • 2102 Views
  • 3 replies
  • 0 kudos