STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

STM32WB - PLACE_IN_SECTION

Looking at the HearRate Example with RTOS.I see that user app holds all the handlers in :PLACE_IN_SECTION("BLE_DRIVER_CONTEXT") static HRS_Context_t HRS_Context;What is the purpose of this placement?Can it be changed to a simple static?thanks

DS.4 by Senior II
  • 1769 Views
  • 2 replies
  • 1 kudos

Is it possible to get 32bit data from PDM to PCM library?

Hi all,We are using stm32 PDM to PCM library to convert PDM mic data into PCM data. On that we had an option to control the mic gain from -12db to 51db as mentioned in data sheet.So we try to increase the db level, But we cannot able to increase the ...

PR.6 by Associate II
  • 3996 Views
  • 3 replies
  • 0 kudos

STM32WB flash size

Hi. I started a new project with the STM32WB35CEU as the target. Both in the datasheet and cubeMX MCU info it states 512Kbytes FLASH and 96KBytes of RAM.But when I generate that project code with cubeMX the linkerscript shows 256KFLASH (rx)  : ORIGIN...

lizerd by Associate III
  • 2305 Views
  • 1 replies
  • 1 kudos

About I2C communication using STM32WL. STM32WLを使用�?��?�I2C通信�?��?��?��?�。

I want to use RTC (RX-8571) for I2C communication with STM32WLE5JC. I wrote the code using [HAL_I2C_Master_Transmit] and [HAL_I2C_Master_Receive], but I can only send the device address of the first byte. The errata says "Write the first data in I2C_...

Resolved! STM32CubeMX , how to live with it

I'm trying to set configuration for STM32WL55JC but I have no luck at all. I have set some pins, namely inputs: PB1,PC6,PC13, outputs: PB10,11,15, pc3,4,5, but the problem is all the time, I'm trying to not to touch almost anything wht is not needed...