STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

STM32WB55 locking up when characteristic value is altered

Hello,I am developing a system using an STM32WB55 Nucleo, such that the STM32 receives data from a Windows application via BLE changing of characteristic value, the STM32 then sends this over uart to an external device which returns an acknowledgemen...

OCatt.1 by Associate II
  • 1248 Views
  • 0 replies
  • 0 kudos

STM32WL55CCU6 - QFN missing VR_PA

Hello,I build my own end node based on STM32WL55CCU6 in the QFN package.During bring up I noticed missing VR_PAVDDPA is available on pin 25.Can someone help me to understand why is missing? I check also on the oscilloscope and is missing too. Nothing...

0693W00000GYKtXQAX.png
MWoło.2 by Senior III
  • 1263 Views
  • 2 replies
  • 0 kudos

How to update beacon data on STM32WB55?

I have created a project in CubeMX with CubeWB. Set the device to beacon mode (UID). On initialization, I can set the NamespaceID and BeaconID. But I do not understand how I can change this data during the operation of the beacon. Please tell me the ...

NKcin.1 by Associate
  • 957 Views
  • 0 replies
  • 0 kudos

BLE disconnection issue on STM32WB5MMG

I am using BLE peripheral on STM32WB5MMG module. For some reason the BLE gets disconnects on its own and not able to connect it again when it disconnects on its own. So I want to understand on what event BLE gets disconnects. Is it anyway possible to...

0693W00000FDrOCQA1.jpg
Gk.1 by Associate II
  • 2920 Views
  • 3 replies
  • 0 kudos

STM32WL55CCU6 : how to receive Uart1 data

Hi I am testing STM32WL55.I am testing UART1 of STM32WL55 by referring to SubGHz_Phy_PingPong​I can transmit data using UTIL_ADV_TRACE_Send.​I tried to receive data from terminal using UART1.But it didnot work.​I inserted UTIL_ADV_TRACE_StartRxProces...

Resolved! PM0271, Rev 3, errata and formula?

Hello ST - would you please clarify these two errata and share the missing formula from PM0271:Slot guard time (1.25 ms or 1.5 ms?The last sentence of 5.2 specifies a 1.25 ms guard time.5.2.2 specifies a 1.5 ms guard time and Figure 22 shows 1.5 ms g...