STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 232 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4076 Views
  • 0 replies
  • 3 kudos

STM32WL matching circuit included in the chip ?

Hello, I am very interested in using the STM32WL for a wireless application. Is the matching circuit already included in the chip (so I just have to add an antenna) ? I don't find any information about this.Thanks.

emil28 by Senior
  • 9718 Views
  • 14 replies
  • 0 kudos

Wireless Sensor Network. STM32F746-DISCO & P-NUCLEO-WB55.

I am currently trying to create a wireless sensor network using STM hardware and ZigBee.I'm new to this type of development and I'm struggling to figure out what hardware I need.I currently have a STM32F746G-DISCO MCU, I would like to use this board ...

RMcNa.3 by Associate
  • 959 Views
  • 0 replies
  • 0 kudos

NUCLEO-WL55JC1 join failed when connecting to The Things Network (TTN), but TTN Console accepts the join request

I am running the LoRwWAN_End_Node example on the NUCLEO-WL55JC1 I've followed the steps set out in the following video:https://www.youtube.com/watch?v=8KNfrWoa1fwI am connecting to an existing local gateway on the TTN, and not using my own gateway as...

0693W00000GZ6tQQAT.png
MMcal.11 by Associate
  • 1934 Views
  • 1 replies
  • 0 kudos

On RX Framing error, UART_DMAAbortOnError can corrupts ongoing TX transfer resulting in 65536 bytes transfered. HAL bug ?

Hi,I use STM32Cube_FW_WB_V1.12.1 on a STM32WB55, with generated init code and HAL functions.I have setup a circular DMA for RX of UART1 and use HAL_UART_Transmit() when I need to send data.I'm communicating with a device (GPS module) that can be conf...

NSAUG.1 by Associate III
  • 1242 Views
  • 0 replies
  • 1 kudos