STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

using Eddystone TLM ADV frame but always shown as URL frame

Hello,I'm working with the Nucleo board the STM32WB55 and i'm trying to send temperture data as in the eddysone tlm frame. But even I've configured the code as EddystoneTLM in the app_conf.h it is always showing up as URL beacon insteade of TLM.Can a...

BLiwa.1 by Associate II
  • 1446 Views
  • 5 replies
  • 0 kudos

Resolved! STM32WB55 QSPI and DMA

I have a custom board with a quadSPI chip installed. I can program a 256-byte page just fine using HAL_QSPI_Transmit(), which I'm monitoring with a logic analyzer. But when I try to do this with HAL_QSPI_Transmit_DMA(), nothing happens on the line...

Storing BLE Bonding Information/Keys on External Flash.

Hello, I am building an application using STM32WB55 ( 1 MB Flash) series microcontroller and planning to use BLE 5.0 to make secure connection with a device. In our use case, I am trying to compute how many keys/Bonding Info can be stored to speed up...

Amogh by Associate III
  • 1771 Views
  • 1 replies
  • 0 kudos

Resolved! How to get low current with STOP2 using STM32WB5MMG.

In STOP2 mode, the current of STM32WB5MMG is around 170uA at 3V.Using the same FW (based on the HeartRate example), the P-NUCLEO-WB55 can achieve a low current (approximately 3 uA).Is there any additional settings for STM32WB5MMG?

TK by Associate
  • 1848 Views
  • 2 replies
  • 0 kudos

STM32WB55VGQ6 wiring without RF ?

Hello,I plan to use a STM32WB55VGQ6 for a project without RF because of components shortage. I read the datasheet and I couldn't find any information about the MCU wiring when there is no antenna connected to it. Do you know if I have to let the RF1 ...

JMARC.11 by Associate
  • 1531 Views
  • 4 replies
  • 1 kudos

Resolved! 1.8V GPIO on STM32WB55 Nucleo Pack

Is there a way to use 1.8V NAND Memory Chip using Quad SPI GPIOs in STM32WB55 Nucleo Pack?   I already wired-up the 1.8V NAND chip and connected to Quad SPI pins of the Nucleo Pack, but I haven't powered this board up yet.

AVILL.3 by Associate II
  • 3618 Views
  • 6 replies
  • 0 kudos

How can I implement BLE Mesh library?

Hello. I know this is a stupid question, but I am not able to find the way to download the ble mesh library for stm32wb55 and inlcuded in a project.Thank you

CGali.2 by Associate III
  • 1169 Views
  • 1 replies
  • 0 kudos