NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I've hit the limit of my research and don't have any experience writing to flash other than at compile time using the keyword 'const', but that doesn't help me because I need to be able to continuously write data. I have a very basic and general sens...
HI all,I’d like to create a system communication using LoRa protocol between 2 devices, I don’t want to use TTN. I’m newbie with LoRa I’ve seen Seed provide SDK to use LoRaWAN but I don’t want to use gateway or server. To be simple I have one device ...
So, I have TIM2 setup to trigger an ADC conversion and the DMA moves the samples out to RAM. I want to do this every 100us for 1000 iterations. Sounds pretty straight forward. There are 3 ADC channels being sampled using the sequencer on every tri...
Hi all,I've been trying to use the STM32WB55 Dev Kit and if I generate the project with the peramitirs below and then try to build the project I get this error;*** Error Code *** C:/Users/bryce/STM32CubeIDE/workspace_1.3.0/STM32WB55-MB1355C/Debug/....
Hi St forum I'm in the progress of creating a peripheral BLE application using the STM32WB55CE on a custom board. I'm trying to implement low power now, but struggling.. Using the X-Nucleo-LPM01A power monitor board I've measured my current con...
In STM\STM32Cube_FW_WL_V1.2.0\Projects\NUCLEO-WL55JC\Applications\LoRaWAN\LoRaWAN_End_Node\LoRaWAN I cannot find an explanation for the NUCLEO-WL55C1 LEDS GREEN, BLUE, RED meanings. In lora_app.c I found: AppLedStateOn = appData->Buffer[0] & 0x01; th...
We want to transmit audio over Bluetooth.We are new to audio and Bluetooth. We have got P-nucleo-WB55 board for Bluetooth and ST EVAL MIC007V1 sensor for digital audio.Can anybody guide us with an example project using I2S.Thanking in advance.
Hey,unfortunately the dongle is no longer recognized as a serial port when i load one of my projects onto the device. When I use the example applications, it works fine. Any idea what this could be.Thanks in advanceEddy
Errors occurred during the build.Errors running builder 'CDT Builder' on project 'EN_Silva'.A resource already exists on disk '..../Debug/sources.mk'.A resource already exists on disk '..../Debug/sources.mk'.A resource already exists on disk '..../De...