cancel
Showing results for 
Search instead for 
Did you mean: 

Can STM32WB55 realize multiple device connection?

Mokail
Associate II

​I want to find a similar code but I can't find it:loudly_crying_face:

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Remi QUINTIN
ST Employee

​I would recommend you have a look at the BLE_p2prouter project under STM32Cube_FW_WB_V1.10.0\Projects\P-NUCLEO-B55.Nucleo\Applications\BLE\BLE_p2pRouteur directory. The BL stack can support up to 2 centrals + up to 6 peripherals in //.

In this project the router device connects to 6 peripherals to get data and transmits the data to a mobile phone  (as central).

AMart.18
Associate

Hi, I tried to connect to 2 centrals simultaneously, but I couldn't do it with the BLE_p2pRouter example. I read documents PM0271 and AN5270, but I couldn't implement the ideas changing the times. What can I do?