STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

Lora AppKey Auto generate

Hello,I'm trying to auto generate the the AppKey on device boot using the KMS Derive.I have enabled the LORAWAN_KMS definition as described on the AN5406 and also the configuration that needed. But the device don't generate any key and after investig...

Spurious conducted emissions for TX(STM32WLE5CC6)

Hello,I have started to develop one LoRa end node around a STM32WLE5CC6 chipset(QFPN48).My device is operating in EU868 band. While the device is transmitting, I acquire the data for the frequency spectrum with a spectrum analyzer. As you can see fro...

0693W00000KbxskQAB.png

Doubts about how to form a pre-defined Zigbee network

Hi,Currently, I'm working with the P-NucleoWB55 evaluation kit, and I'm developing a Zigbee network to exchange some messages between devices. My problem comes when I have to form and join the network. I'm not sure about the meaning of the configurat...

Pablo1610 by Associate II
  • 2655 Views
  • 1 replies
  • 0 kudos

How do I disable Zigbee security level?

I am using STM32WB Discovery kit for STM32WBB5MM MCUs for development. I've setup the board as a RFD, Centralized End Device. How do I disable Zigbee security level if I don't need it? Currently, I have to set it manually in APP_ZIGBEE_NwkForm() by  ...

VWu.1 by Associate
  • 1228 Views
  • 1 replies
  • 0 kudos

STM32WL with the LoRaWAN and the Sigfox coexistence

Hello, I would like to use the NUCLEO-WL with Sigfox and LoRaWAN in the code as proposed in the workshop (youtube video : MOOC - STM32WL workshop - 6 LoRaWAN and Sigfox coexistence). However, the zip project is not part of CubeWL. Thus, How can we up...

LLr.1 by Senior
  • 843 Views
  • 0 replies
  • 1 kudos

IEEE 802.15.4 BEACON Mode

Hello ST Community​,​I want to know if the STM32WB55RG supports MAC 802.15.4 Beacon Mode.​For now, I'm sure that the CM0+ Stack supports Only the Non Beacon Mode (SO=BO=15) and Full broadcast Mode (PANID 0xFFFF​, dest @ 0xFFFF) and OFC doesn't suppor...

MYous.3 by Associate II
  • 1229 Views
  • 1 replies
  • 0 kudos