NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello Everyone,Intro. Our embedded project was defined based on the BC127 Bluetooth module, which enjoyed Melody 7.0 firmware. We used the SPP protocol in such a way that a new virtual comport is added to my device manager list when the operating sys...
HiFor the past few days I've been trying to get a dual core project with FreeRTOS and the LoRaWAN Stack for a custom STM32WL55 design to work but the CubeIDE seems to not properly generate everything that's required for it to work.When blindly genera...
Hi Im looking for he hands on application for the "mooc - stm32wl workshop - 4 point" as on you tube https://www.youtube.com/watch?v=n7OoTStkczs . Anyone got a link to where I can get the exact same applications?Many ThanksScott
arm-none-eabi-gcc -o "LoRaWAN_End_Node_DualCore_CM0PLUS.elf" @"objects.list" -mcpu=cortex-m0plus -T"/Users/ben.blouin/dev/LoRaWAN_End_Node_DualCore/STM32CubeIDE/CM0PLUS/STM32WL55JCIX_FLASH.ld" --specs=nosys.specs -Wl,-Map="LoRaWAN_End_Node_DualCore...
Hi Im using the SUBGHz in Lora mode for communication with point to point. What I want to do is design low power communication. I plan to send the first packets from the battery node to SF12 , then the permenant connection node will detect the sign...
I am currently using NUCLEO-WL55JC board. However, I could not initialize the logic analyzer.The watch tab works well, but the analyzer window seems not working. And, I have an error at the bottom showing "Trace: No Synchronization". I set the core f...
I am using the Lora-e5 with the STM32WL55x . I am designing point to point systems and setting them as Lora comms. The application uses various SubGHz commands that I have linked in from the library, like SUBGRF_WriteRegister(..) etc. Is there any do...
Hi everyone,I'm developing a device based on a STM32WB55 which has a USB interface. Using CubeMX I created a project with a Custom HID device, FreeRTOS + CMSIS v2.I need to send frames of a proprietary protocol which content usually don't exceed 64 b...
@file stm32wbxx_hal_qspi.hQSPI_CommandTypeDef -> DdrHoldHalfCycle#define QSPI_DDR_HHC_ANALOG_DELAY#define QSPI_DDR_HHC_HALF_CLK_DELAY ((uint32_t)QUADSPI_CCR_DHHC)