STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 234 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4077 Views
  • 0 replies
  • 3 kudos

I'm having issues with the DMA Callback functions never being called after triggering the "HAL_SAI_Transmit_DMA" function.

Situation - I'm combining code examples from the STM32WB Opus Library code, with that of the Echo Cancellation (AEC) Function Pack. Using the code base to have support for a microphone, speaker, and Bluetooth. When implementing the code for the CCA01...

STM32WL55JC1 LoRa Timeout Issue

We are also facing same tx timeout in our custom designed hardware. We are using XO clock in the design and donot have option for TCXO. Please share your inputs whether STM32WL55JC1 will work with XO clock. We got struck with TX Timoeut issue.

0693W00000JNQ9LQAX.png
HVeer.1 by Associate II
  • 3361 Views
  • 5 replies
  • 0 kudos