NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I am using the LoRa Development board B-L072Z-LRWAN1 and it has got STM32L072CZ microcontroller and want to write FUOTA service using LORAWAN
error: no stm32 target found Stlink is ok ,i can download program to another board. As manual's configuration, I configure MB1355C(P_NNUCLEO_WB55), I can't enter dfu mode. But the usb dongle is ok. So i think usb driver is ok.There is a 'FAIL.TXT' ....
Hi,I have designed two PCBs that use STM32WLE5C8U6. I am experiencing range problems. The communications does not exceed 15 meters of range. What is the expected range? Below is what I use to initialize the radio. I have an R0 so that I switch betwee...
Hi, my name is Jorge.I'm currently working with an STM32WB5MMG, which has Bluetooth LE 5.2 connectivity. In the current version of the project, it's working with two Bosch sensors. The BMI088 with accelerometer and gyroscope, and the BMM150 with a ma...
Hi,I have a wb55 nucleo and a wb55 usb dongle. The usb dongle is running zigbee onOff Server example code. However, it is using install code instead of preconfigured link key as shown below./* Using the default HA preconfigured Link Key */ //memcpy(c...
My purpose is to be able to send and receive serial communications using USART in asynchronous mode.When I try to adapt these kind of examples using UART_DMA in FreeRTOS, are not working. I copied the configuration regarding IRQs, DMA and USART inici...
Hi! I started testing sound transmission to a smartphone using BlueVoice and noticed sound distortion.When recording speech, there are distortions, but they are not very noticeable. To check, I placed a speaker near the microphone and connected it to...
Hi,Currently looking into having multiple multicast groups on an STM32WLE5, using the LoRaWAN middleware included with STM32Cube_FW_WL_V1.2.0 package. When looking at "LoRaMacTypes.h" (in Middlewares/Third_Party/LoRaWAN/Mac), I came across the const...
Hello guys,I want connect to a bluetooth device/beacon from STM32WB.I've used this function to setup the connection with the device found when scanning but it won't connect to it it always print out "[BLE] Successfully Connected to Slave" and then ...
this error showed when i build the project ```c:\st\stm32cubeide_1.8.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: C:\Users\gjallouli\STM32C...