STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

How to create a custom Bluetooth Service?

I have a custom board using the STM32WB55RCV6, I am able to generate a project that advertises the correct Bluetooth name, but I cannot connect to it. I have looked at several projects online and compared my STM32CubeMX IOC file to theirs and I do no...

MStar.3 by Associate
  • 2114 Views
  • 3 replies
  • 0 kudos

Whether STM32WL will support CAN protocol interfacing?

I 'am new to STM32WL & CAN protocol interfacing! I'm currently working with the STM32CubeMX platform & some examples are given for CAN interfacing for other variants of STM32 MCUs.But there is no CAN interfacing option available in STM32WL. So I'm un...

Ppk.1 by Associate II
  • 2598 Views
  • 2 replies
  • 0 kudos

What is the value of LPTIM_CNT after MCU RESET?

Hello ST microelectronics support team.I'm developing an IOT application using the STM32WLE5CC for gas measurement. To measure the pulses I'm thinking of using the LPTIM, but I have a doubt.In topic 26.4.14 of the RM0461 reference manual, I became aw...

Takahashi by Associate II
  • 2157 Views
  • 3 replies
  • 0 kudos

Changing RF Frequency at runtime.

Hi,Is there any side effects of changing the RF Frequency of the Lora Modem during runtime.Radio.SetChannel(RF_FREQUENCY);Can this be used to change the frequency at runtime? Thanks

MCarl.7 by Associate II
  • 1762 Views
  • 2 replies
  • 0 kudos

Problem loading stack on a nucleo STM32WB55

It's a board I've been using for a while, and I'm struggling loading a new stack onto it.Here are the steps I've executed:1/ powercycle2/ start FUS3/ delete image4/ powercycle5/ start FUS6/ get FUS info: FUS_IDLE | FUD_NO_ERROR | Version=1.1.1.0 | st...

OTOMA.2 by Associate II
  • 5884 Views
  • 18 replies
  • 0 kudos

P_NUCLEO_WB55(stm32wb55rgv6) Help!

error: no stm32 target found Stlink is ok ,i can download program to another board. As manual's configuration, I configure MB1355C(P_NNUCLEO_WB55), I can't enter dfu mode. But the usb dongle is ok. So i think usb driver is ok.There is a 'FAIL.TXT' ....

Lep by Senior
  • 2674 Views
  • 5 replies
  • 1 kudos

Increasing the range of STM32WL devices.

Hi,I have designed two PCBs that use STM32WLE5C8U6. I am experiencing range problems. The communications does not exceed 15 meters of range. What is the expected range? Below is what I use to initialize the radio. I have an R0 so that I switch betwee...

0693W00000NpxZdQAJ.png
MCarl.7 by Associate II
  • 2694 Views
  • 3 replies
  • 0 kudos

BMM150 causing problems with the BLE communication

Hi, my name is Jorge.I'm currently working with an STM32WB5MMG, which has Bluetooth LE 5.2 connectivity. In the current version of the project, it's working with two Bosch sensors. The BMI088 with accelerometer and gyroscope, and the BMM150 with a ma...

jorgazam by Associate II
  • 4411 Views
  • 6 replies
  • 0 kudos