STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

How to configure BLE from STM32U5 MCU pinout (IOC file)?

Hello! The title pretty much says it all - I'm trying to figure out how to configure BLE between two B-U585I-IOT02A boards, but establishing the BLE connection is a bit confusing to me. Am I able to configure it from the UFBGA169 IOC file in STM32Cub...

juyec by Associate II
  • 4711 Views
  • 6 replies
  • 0 kudos

Resolved! STM32WB55 USB CDC Transmit always return USBD_BUSY

I have setup USB connectivity between the STM32WB55 Nucleo board and my pc.As I connect to the board, my application sends some data and the board response accordingly. I can send another command to start the application running on the hardware, whic...

LHans.2 by Associate II
  • 2915 Views
  • 2 replies
  • 1 kudos

Resolved! Wireless stack and FUS image addresses for upgrading

Hello.I'm planning a project that will use large amount of flash memory, therefore, I will need to be cautious with memory saved for app updates. I'm using STM32WB55VGQ6 with 1MB of flash memory on custom designed board. my current application is abo...

YWor.1 by Associate III
  • 6258 Views
  • 13 replies
  • 0 kudos

Resolved! STM32WLE Standby Mode - Unresponsive at Low Voltages (<2.15V)

Hi there,I am using an STM32WLE with an input voltage range of 2 - 3.3V. It will eventually be powered by a lithium coin cell, but I am currently using a benchtop power supply. The datasheet states that both the MCU and the radio should function down...

RLind.3 by Associate III
  • 2118 Views
  • 4 replies
  • 0 kudos

Using STM32WB55 BLE Heartrate example as start point then adding I2C functionality to read sensor but second I2C exchange (e.g. read) causes code to hang in HW_TS_RTC_Wakeup_Handler().

Working on project with BLE interface and need to add I2C interface to read a sensor. Started with BLE Heartrate example (it wakes up ever 1s which I also need to do) and added I2C by using CubeMX to generate the new code. To start testing I added th...

MMcke.1 by Associate
  • 2140 Views
  • 3 replies
  • 1 kudos

COMP1 HW or SW problem recovering from STOP2 mode

Hello everyone,​I discovered a problem with the STM32WLE5CCU6 using the comp1 on stop2 mode.​More specifically, when the debug is enabled on stop2 mode using the command HAL_DBGMCU_EnableDBGStopMode() the comp1 is working and I get all the peaks of t...

0693W00000Nr9LfQAJ.png 0693W00000Nr9LpQAJ.png 0693W00000Nr9NlQAJ.png

STM32 BLE

Hello everyone,We are planning to use ST products in our new BLE-supported projects. But I am not sure which product is suitable for this.As I see, there are some BLE chips connectable with SPI and there are SoC ICs like STM32W.I am not sure which is...