STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 277 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4103 Views
  • 0 replies
  • 3 kudos

Resolved! Missing command ACI_HAL_TONE_START in BLE full stack 1.13.3

Hello,From 1.13.0 to 1.13.3, the command ACI_HAL_TONE_START was removed (get Unknown command return). The release note indicates that some HCI commands were removed not ACI commands.Is it an error or should we prepare to move to the full extended sta...

AnthonyS by Associate II
  • 2661 Views
  • 5 replies
  • 0 kudos

[STM32WLE5CC] Firmware behavior according to power

Currently, we are using the STM32WLE5CC MCU.Some MCUs do not operate normally when the same firmware is inserted into several MCUs. (Abnormal current, delays in Uart log output, RF is not transmitted)If a higher voltage (4.4V) than the MAX operating ...

BHwan.2 by Associate
  • 1506 Views
  • 1 replies
  • 0 kudos

Why my HS_STARTUP_TIME is so high?

Hello,I'm doing a new board bring-up and following the document AN5503 (https://www.st.com/resource/en/application_note/an5503-bringing-up-the-bluenrglp-bluenrglps-devices-stmicroelectronics.pdf)At chapter 4 (HS_Startup_time) I use the example firmwa...

0693W00000QKYDrQAP.png
jbie by Associate II
  • 1443 Views
  • 1 replies
  • 0 kudos

Making BLE Application lossless on STM32WB5MMGH

We have implemented BLE application on STM32WB5MMGH. I see that some of the BLE packets are getting lost in transit. The peripheral and the master are in very close proximity. I understand that packets can get lost depending on environment but my que...

SA.14 by Associate
  • 1069 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.