STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

STM32WB55 DFU problem (can't detect by laptop) !!!!

I designed a custom board with STM32WB55 with a USB connection to update the BLE stack in DFU mode.When I connected the board to my laptop's USB port, it appeared in the device manager and was detected as a USB device, however since yesterday when I ...

SFall.1 by Associate
  • 1405 Views
  • 1 replies
  • 0 kudos

NUCLEO-STM32WB15 HardFault Error with BLE custom Template.

Hi,I have a problem when I try to develop a program with STM32IDE for my NUCLEO STM32WB15. I want to use the BLE with a custom template but unfortunately, after launching the program I get a HardFault Error (I guess from the RTC).According to my rese...

0693W00000QKx5sQAD.png 0693W00000QKx5iQAD.png 0693W00000QKx6CQAT.png 0693W00000QKx6RQAT.png
ET_FR by Associate
  • 1579 Views
  • 1 replies
  • 0 kudos

cannot find boards on ST BLE Mesh

**English is not my natural language, sorry for my poor English.Hi, I'm beginner to STM32.I use WB55 boards to connect ble mesh. I used the example code in STM32 CubeIDE (BLE_MeshLightingPRFNode). However, application in phone(ST BLE Mesh) rarely fin...

mpark.1 by Associate
  • 1536 Views
  • 2 replies
  • 0 kudos

After initialization, I2C is always busy

I am using the Nucelo board and communicating with an IKS02A1 trough I2C2 using PINs PA11 and PA12 with the following configuration: I have initializaed the I2C folowing the guidelines in "stm32wlxx_hal_i2c.c", and when I use "HAL_I2C_IsDeviceReady()...

0693W00000QL5xUQAT.png 0693W00000QL6HAQA1.png 0693W00000QL6PhQAL.png
AZube.2 by Associate III
  • 2479 Views
  • 6 replies
  • 0 kudos

Resolved! STM32WB55 Ram Memory Size

Hello guys, how are you?​I'm investigating some .bss overflows i'm facing and i ended up on some weird question. Linker file for STM32WB generated by CubeMX is as follows:RAM1 (xrw) : ORIGIN = 0x20000008, LENGTH = 0x2FFF8RAM_SHARED (x...

MBuen.1 by Senior
  • 2520 Views
  • 1 replies
  • 0 kudos