NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I have an STM32WB that is configured in central, it connects to 8 devices in peripherals mode at the same time. This configuration works well, but from time to time the BLE stack does not respond, I see 8 peripherals disconnected and I do not receive...
Hi community,I have devices with own firmware in which I use also the BLE_OTA app with slight modifications to upload updates to my own firmware. Initially I used the app from ST to update the firmware. Then I created a tool in Python for Windows, Li...
Is the ble server notification interval at least 7.5ms?Can I reduce it?If the throughput is not enough and the notification interval can only be as low as 7.5ms?Am I the only way to increase the amount of data per notification (for example, from 15by...
Hello, I recently bought an STM32WL55JC2 board (nucleo). I have downloaded the STM32 IDE.When I connect the card in USB directly to my pc there are three LEDS that blink successively (red green blue).I can build my project (empty) on STM32IDE on both...
I want to use an external multiplexer to increase the number of ADC but switching speed is one of concern.Fortunately, some multiplexer has a 13 ns switching speed (~100 MHz) and I'm planning to switch it using a GPIO signal.However, it arises concer...
I would like to know if I can use X-NUCLEO-CCA02M2 to input speech audio and X-NUCLEO-CCA01M1 for speech audio output?
I use my own board (as ble server) to notify the client, each notification is 120 bytes, I found that I can only transmit 30 per second. Actually my requirement is 100 transfers per second.Do I need to modify anything?