User Activity

I am using 2 Uart with interrupt function. I have enabled two interrupts at the same time. But I can access only one Uart at a time. Another Uart interrupt is no response.Kindly support for rectify this issue.
Hi, We are trying to configure device keys using AT commands. We are able to change the App EUI and Device EUI using AT commands. But we are facing issues when modifying the App key and NWK key using AT commands. We referred the AT commands configu...
Hi,Now I am working on I2C sensor (BH1750 sensor) integration with LoRaWAN base firmware(STM32cube_FW_WL_V1.0.0) in RAK module. The controller specification is STM32WLE5JCI had configured the I2C peripheral initialization as mentioned below document....
Hi,Once I flash the base firmware(STM32cube_FW_WL_V1.0.0) in the RAK3172 module, I view the serial print. It displays Europe frequency… then I open the firmware(STM32cube_FW_WL_V1.0.0) and check the file named lora_info.c… in the file Europe and US r...