STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 132 Views
  • 0 replies
  • 0 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4029 Views
  • 0 replies
  • 3 kudos

Long Characteristic Write Value

Just trying to figure out the max size I can pass to the write function.According to AN5289 :Write long distant value aci_gatt_write_long_char_value(conn_handle, RxCharHandle,offset, chunk_size, (&payload)+offset) Max data write length is 243 bytes.I...

DS.4 by Senior II
  • 1080 Views
  • 1 replies
  • 0 kudos

STM32WB15 Wake_up pin polarity issue

Hello,I use a stm32WB15 MCU in shutdown mode with a wake up by the wake up pin PA0 (System wake-up 1).Everything works fine with the polarity "High". I use the HAL function "HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1_HIGH)".But with the polarity "Low" a...

JGuir.1 by Associate II
  • 3071 Views
  • 4 replies
  • 0 kudos

Resolved! Stm32 default clocks after reset/boot?

Hi, I am trying to understand the startup process of stm32 mcu. So I have a good knowledge with STM32 and HAL but I want to learn a little deeper with the registers.So I created a blank project and included only the peripheral header file (stm32wb55x...

suads by Associate III
  • 8283 Views
  • 3 replies
  • 2 kudos

STM32WB55: Trying to get the RTC running based on HSE_DIV32

Hi,I have been trying to use the HSE_DIV32 clock as input for the RTC but without success.I cannot find any example where this is done even though it's available in the datasheet and the register map.I have been doing this after enabling the HSE cloc...

apous.1 by Associate II
  • 1348 Views
  • 2 replies
  • 0 kudos