STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 222 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

How do I toggle a pin upon each BLE packet.

I'm using the STM32WB55, with STM32CubeWB V1.14.1 & `stm32wb5x_BLE_Stack_full_fw.bin` V1.14.1.Looking in `app_debug.c`, I can configure `aGpioConfigList[]` and `aRfConfigList[]`, which allows for CPU2 to toggle a GPIO pin based on various events.I ca...

Olly by Associate II
  • 1423 Views
  • 1 replies
  • 0 kudos

Resolved! Where to find fuota_automation.py from AN5554 document

Document AN5554 Rev4(LoRaWAN® firmware update over the air with STM32CubeW) mentions, on page 60, about file fuota_automation.py. I can not find this file in software package for STM32WL. Is this file accessible to download?

MZapa.2 by Associate
  • 1236 Views
  • 1 replies
  • 1 kudos

How to receive SPI data from MAX31855 with Nucleo WB55 ?

Hello, I use a Nucleo WB55 and I would like to receive temperature data from MAX31855. The protocol used is SPI. 1) ConnectionsFirstly I tested the MAX31855 with an Arduino and I managed to get data. I used the same MAX31855 and double-checked the wi...

0693W00000Y7TCrQAN.png 0693W00000Y7TG3QAN.png 0693W00000Y7THuQAN.png 0693W00000Y7TNYQA3.png
LVolp.2 by Associate II
  • 2482 Views
  • 1 replies
  • 0 kudos

Resolved! Do I need a new RF CERTIFICATION of the STM32WB5MMG on a custom pcb with body distance LESS than 20cm?

In the datasheet of the STM32WB5MMG Module is writtenThe module antenna must be installed to meet the RF exposure compliance separation distance of “20 cm�? and any additional testing and authorization processes as required.in the sections FCC and IS...

BGeig.3 by Associate II
  • 1357 Views
  • 1 replies
  • 1 kudos

BLE stack questions regarding connection and advertising

I have some question related to the BLE stack code. Specifically regarding GAP operation.My device is the peripheral.On first connection to my device from peer :How long can a 'connection procedure' take. From when the stack is receiving a connection...

DS.4 by Senior II
  • 1054 Views
  • 1 replies
  • 0 kudos

Problem LoRaWAN EU868 certification in Ukraine

Hi everybody,I have to problem with LoRaWan EU868 certify in Ukraine, specifically as follows:I am using ABZ module as CMWX1ZZABZ-091 to develop product, and I set ABZ module such as:+ firmware based on source code en.i-cube lrwan v1.3.0+ used Lora m...

npham.1 by Associate
  • 1789 Views
  • 1 replies
  • 0 kudos