STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! SYSCLK vs SystemCoreClock

Hello,I want to know difference between SYSCLK and SystemCoreClok.When ı try to configure clock of different peripherals I saw terms SYSCLK and SystemCoreClock. I use MSI for SYSCLK which is configured to 32MHZ and for cpu1 ı divided sysclk by 4 and ...

MOB1 by Associate II
  • 3913 Views
  • 2 replies
  • 0 kudos

Resolved! STM32WB55 enable IPCC chage clock and broken usb

I'm generating code with STM32CubeIde 1.11.0 for a STM32WB55, in my test project there is an USB CDC and BLE is enabled.When I enable BLE also IPCC must be enabled, but after HW_IPCC_Init is called usb clock is wrong so my usb device doesn't work any...

juvann by Associate III
  • 2412 Views
  • 4 replies
  • 0 kudos

Resolved! STM32WB BLE OTA low upload speed on some phones

Hello,I am using BLE_OTA project for STM32WB55. I upload a bin file which is 350 kb using ST BLE Sensor. However, the upload speed is so lower for some phones. For example, it takes up to 450 seconds on some android phones while the others take 25 se...

serhat by Associate II
  • 1520 Views
  • 2 replies
  • 0 kudos

Resolved! STM32WB55 BLE_Ota erasing the flash when upload is started

Hello everyone, I'm using BLE_Ota application for STM32WB55 (https://github.com/STMicroelectronics/STM32CubeWB/tree/master/Projects/P-NUCLEO-WB55.Nucleo/Applications/BLE/BLE_Ota) I can able to run the code successfully. In the OTA code, it erases the...

serhat by Associate II
  • 1487 Views
  • 2 replies
  • 0 kudos