cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB Dongle stop working

PGarg.1
Associate II

I Have updated the Dongle's fuses to 1.2.0 version. I did a successful test with the example of transparent mode and the monitor RF. Now I'm trying to use it as Server in a p2p example and it doesn't works. To discard, I flash it again with the example of the transparaent mode and I now I can't conect with monitor RF giving me the following pop-up.

0693W00000NrXARQA3.pngIs it that the Dongle is broken? I tryed programming on it the heartrate example and it didn't work.

If I read the fuses it response fine:

0693W00000NrXBUQA3.png 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PGarg.1
Associate II

I solved: I put again the ble stack and it worked. First I put in it an other stack (Zigbee) and then I put it the ble stack again and start working.