STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! STM32 program only read data from sensor once and then freezes

The given example on LoRaWAN_End_Node software pack is transmit temperature, humidity, and pressure data. My main objective is to do the same thing but instead of send those three datas, I want to send the parsed GNSS data like how the SimOsGetPos di...

0693W00000aIihJQAS.png
Wtuya.1 by Associate
  • 2480 Views
  • 1 replies
  • 0 kudos

STM32 and sx1262MB2CAS Shield

Hello thereI am completely new in STM32, I need to use two SX1262MB2CAS shield to tx with one of them and rx from the other one.Do you know which drivers i will need and how to configure the stm32cubeide project to have acces to two stm32?

AMitj.1 by Associate
  • 1392 Views
  • 1 replies
  • 1 kudos

A Hint to Drive the VL53L4CD using STM32WL55JC

Hello, I tested the VL53L4CD with the Nucleo-STM32F401 using the ST-Example and I got Ranging readings. However, when I port the code to use the STM32WL55JC, I always get an I/O Error.I use the same pin configurations to drive the sensor as in the Ex...

0693W00000aIb4ZQAS.png 0693W00000aIazVQAS.png
AElgh by Associate III
  • 1313 Views
  • 1 replies
  • 0 kudos

STM32WB55 Device Name is not changed in GAP/GATT

Hey,I try to change the device name for my broadcast inside the initialization of the Ble_Hci_Gap_Gatt_Init() funtion. My implementation is the following:static void Ble_Hci_Gap_Gatt_Init(void){   uint8_t index; uint16_t gap_service_handle, gap_d...

BSpoe.1 by Associate III
  • 2768 Views
  • 4 replies
  • 1 kudos

STM32WB55RGV6 is not starting up.

We have a product that uses the STM32WB55RGV6 controller. Some of the boards start up without issue, some of them occasionally fail with the STM32WB55RGV6 processor not starting up, and others never start. We don't know if it is a grounding issue wi...

0693W00000aIbxPQAS.png
BBoos.1 by Associate
  • 1460 Views
  • 2 replies
  • 0 kudos

Resolved! STM32WB Openthread logging level does not change

Im using the Thread_Coap_Generic Example for the STM32WB5MM-DK (CUBEWB version 1.15.0). THe CPU2 Binary is as it is descibed in the readme.txt "stm32wb5x_Thread_FTD_fw.bin". I want to change the logging level of the Openthread. The Change of OPENTHR...

CBuch.1 by Associate III
  • 1371 Views
  • 1 replies
  • 0 kudos

Is it possible to brick FUS 1.2?

I had my NUCLEO-WB15CC running stack full v1.15 and today I decided to upgrade it to v1.16 and got "Warning: FUS_STATE_ERR_UNKNOWN". And now I have no stack and I'm unable to install it.And I can't even start FUS, when I try, I get those errors:Error...