NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Here is what I try to do:Imported SubGHz_Phy_PingPong to my workspace.Double click on IOC to launch CubeMX and do simple HW change, in my case enabling EXTIO interruptsAfter code generation there are many compilation errorsCan be reproduced with othe...
Hello All...I have downloaded the X-Cube-EEPROM as I would like to create persistent variables. I have an existing project using Nucleo-WB55. Can someone help defining what files/folders to import from X-Cube-EEPROM into my project and what the file ...
I am using nucleo STM32WB55RG to build an BLE application. I am having a very weird issue.At first I create an BLE application using CubeMX.I used server profile with custom template enabled (You can refer to attached cubemx file .ioc)The application...
Where in the files or a function can I put a character to be read by Android(maybe humidity reading) when using BLE in STM32WB55. I can not find any help from your videos. Please if you reply send me the exact function and include character "thanks"...
Hello,I am developing my own project based on Lorawan_end_node project, i have some doubts regarding to memory addressing. In linker file:/* Memories definition */ MEMORY { RAM1 (xrw) : ORIGIN = 0x20000000, LENGTH = 32K NVM_RAM (rw) : ORIGI...
Before release of package v1.3.0 binary size were <90kb and .ld has 3 partition in memory as below,/* Memories definition */MEMORY{ ROM (rx) : ORIGIN = 0x08000000, LENGTH = 256K RAM1 (xrw) : ORIGIN = 0x20000000, LENGTH = 32K /* Non-backup SRAM1 ...
According to the user manual (st (dot) com/resource/en/user_manual/um2115-discovery-kit-for-lorawan-sigfox-and-lpwan-protocols-with-stm32l0-stmicroelectronics.pdf), you can optionally close SB13 to get a 32MHz clock signal to the MCU instead of attac...
When A/D is set to scan thru a sequence of channels can a single external trigger allow you to go thru the whole sequence or do I need a trigger for each of the channels in the sequence??Been struggling with this for a while and I have some bare bone...
Hello. I am following document:https://github.com/STMicroelectronics/STM32CubeWB/blob/master/Projects/STM32WB_Copro_Wireless_Binaries/STM32WB5x/Release_Notes.htmlon how to flash STM32WB firmwares.I am going through steps:How to flash the Wireless Cop...
The steps performed:First read the FUS version.Selected the FUS bin file to flash.Flashed the above-mentioned file.Then again when I read the FUS version it was displaying as 00000000 in GUI
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.