STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

How to achieve low power Bluetooth advertising with STM32WB

I'm having issues getting the low power sleep to work with Bluetooth enabled on the STM32WBIs there any guide or app note on steps needed to achieve lowest power level BLE advertising?Basically no matter what I do - if I enable bluetooth advertising ...

ChrisLB by Associate III
  • 11020 Views
  • 16 replies
  • 2 kudos

Resolved! STM32WB5X BLE packets sizes

HiI would like to use STM32WB5MMG-DK.1) I tried to program 1.15 software packages for stack-ble + FUS + SAFEBOOT.The stack ble file size is 149KB, according to the release note it suppose to be programmed at address 0x080C5000 (or 0x080CE000).The FUS...

Ofer by Senior
  • 8325 Views
  • 5 replies
  • 0 kudos

Resolved! power consumption in stop modes,standby and shutdown mode

i am trying to measure the power consumption of the MCU in my custom board with different sleep modes, while measuring the stop2 mode i am getting consumption of 110 uA in the datasheet its showing of 2 uA ,even for shutdown and standby mode also its...

sabari1 by Associate III
  • 4033 Views
  • 4 replies
  • 0 kudos

LoRaWAN context management issue

I run a LoRaWAN End Node application on the custom board based on STM32WLCCU6 MCU. Application has enabled contex management to store LoRaWAN data and be able to resume communication after power loss without rejoining to the network. NVM memory is up...

0693W00000WJR75QAH.png
JNowa.4 by Associate III
  • 2359 Views
  • 2 replies
  • 0 kudos

Resolved! I-CUBE-LRWAN for Nucleo-476 ?

why icubelrwan stack does not support stm32f407.How I can use stm32nucleol476rg as lora end node using icubelrwan stack.

Mshin.2 by Associate
  • 2125 Views
  • 2 replies
  • 0 kudos

Resolved! nucleo-wb55rg and uart?

I have the following code where the variable string takes on the float value toPC correctly. I step into the HAL_UART_Transmit_IT and step over all the assignments and all looks fine yet I never see the TDR register update with the first value. Fur...

SWenn.1 by Senior III
  • 1800 Views
  • 2 replies
  • 0 kudos

STM32WB5MMG 1LAYER LAYOUT

HY IT'S MY FIRST TIME HERE ASKING ABOUT STM32WB5MMG MCU CIRCUIT BOARD DESIGNE WITH 1 LAYER :1 - CAN WE ATTACH ALL THE PIN FROM 61 TO 84 TO GND BECAUSE WE DON'T WANT TO USE THIS PINS ?2 - CAN WE PLACE SOME PADS OR SENSOR(IN MY CASE ACCEL GYRO) CLOSE T...