NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi All,Currently I am working on STM32WLE5CCU6 + RAK3172 using STM32CubeIDE. So I am checking sleeping current.Currently I am getting 340uA of sleeping current.I want to make it reach to 4uA.Can anyone guide me how can I achieve that. I have some dou...
I want to know how to design a PCB board about stm32wb55cc serial ic ,and should it need a antenna?If it need, what is the most suitable antenna to the ic?
Hello everyone, I am trying to do tone calculator. I am using DSP , ADC ,DMA and timer for sampling rate. I am using tone genarator and for example if tone is 500 hz and my fftoutbuffer[16] is going high value (noramlly 130 but when tone generate is ...
Greetings,I am working on the LoRaWAN Project and facing issues in updating RTC from a server/UART in LoRaWAN library.My code is getting stuck while updating RTC, I am recieving time and from UART through user input.RTC_TimeTypeDef set_time;RTC_DateT...
Hi all, I am looking for a list of resources (peripherals, memory, etc) that are required by the STM32_WPAN stack implementation for the STM32WBA52. I previously used the STM32WB55 and e.g. AN5289 lists which peripherals are shared with the M0/BLE co...
Just used the example application "LoRaWan_End_Node" with the Nucleo-WLWL55JC board.This example send every 10seconds data to a gateway which is received in the TheThingsNetwork environment. Default is "LoRaWan_End_Node" disabled, when "USE_FULL_ASSE...