NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
We are using the STM32WLE5JCI6 chip and we are mostly done with hardware and software development but got stuck with the below issues.We are trying to read two analog inputs from PB4 (ADC1_IN3) and ADC_CHANNEL_VREFINT. (We are using a Lithium thionyl...
The first time I runned the program it worked correctly but then it doesn't work
Hello,I want to mass erase the flash of the P-NUCLEO-WB55 board using UART and USB in boot mode. I have tried mass erase using the STM32Cube programmer it is showing an error "Mass erase operation failed Please verify flash protection". All the optio...
STLINK-V3PWR Not able to connect to STM32WL and other STM32 MCU's using STM32CubeProgrammerSame MCU is working with STlink-V3 13:39:13 : ST-LINK SN : 002F004D3431510137383732 13:39:13 : ST-LINK FW : V4J2B1P4 13:39:13 : Board : STLINK-V3PWR 13:39:...
Hi all.I'm working with stm32wle5 (rak3172 module) with a custom board.It works but now I need to change default data rate DR_2 to DR_0 (need to increase distance).I have already tried to change the lines below at file RegionAU915.h//Minimal datarat...
Hi,I'm a new user of STM MCUs. I have a custom board with stm32wle5 on it, and I try to config the lorawan to send data to Helium. I searched over the internet, but all the examples are based on the Nucleo board and use a pre-configured .ioc file. Is...
Hi,I followed this setting herehttps://community.st.com/s/article/how-to-configure-the-rtc-to-wake-up-the-stm32-periodically-from-low-power-modesBut still not able to select LSE as RTC source. What steps I missed? Please help.Thanks!
Hello,I have a STM32WLE that works with the lora end_node project I have a sensor that i power up with a mosfet when needed. But during the time that the chip is sleeping i need to disable the internal I2C pullup (+30 uA more due to the fact that th...
Hello, I've begun my learning experience with modification of HRSTM example for STM32WB15. However i seem to have problem with using ADC inside of the task while CFG_LPM_SUPPORTED is set to 1. What can be a cause of such problem?
HiI try to use task on the STM32WB5MMG mcu.My task check if a queue is not empty, if not empty then copy the item on its top and send its message by the BLE. The task handler is:void ble_tx_messages_queue_handler_task(){ queue_element *element; Circu...