User Activity

When plugging in a device in DFU mode to a native USB port of the notebook cubeprogrammer reports:When using it over USB HUB or other port the Cubeprogrammer works fine (we never activated RDP).USBDeview shows no difference in the installed drivers. ...
I'm playing with the above mentioned example using the WB55 nucleo board.When using a Samsung S10 on android with BLE Toolbox from STMicro we can reach 100-160kbyte/s throughput.When using a HP notebook with builtin or TPLink/ASUS bluetooth dongle th...
Modified the BLE_Throughput example to use indication characteristics instead of the notification.I also set the interval to 1 second for debugging purposes because I saw that only 1 IND is read by the client per connection interval.I see that SendDa...
I just started with the 2x P-NUCLEO-WB55 board.Upgdated the FUS using the Cubeprogrammer and flashed the BLE_LLD then BLE_FULL staks, at least on one board. The other board was not reachable via USB after FUS update. The wireless page is not availabl...
Kudos from