Does ST plan to support Matter? Are there any code examples or application notes available (I couldn't find any). Also, specifically, will a single STM32WB55 be able to support Matter connectivity and provisioning (seems like it should).Thanks! Dan.
The documentation for the IHM15A1 dual DC brushed motor driver board (p.2) says it is only compatible with the following Nucleo boards: NUCLEO-F401RE, NUCLEO-F334R8 or NUCLEO-F030R8.
I have a Nucelo-WB55RG. Can I use the IHM15A1 with it? Does the d...
Yes - that was my impression, that I could use any Nucleo board that could provide this minimal set of control signals. So you don't see any inherent reason why it couldn't work with the Nucleo-WB55RG - right?