STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

STM32WB55 power consumption

Hi,I have a board which has a STM32WB55RGV6 MCU and i have a problem. When i connected my board to Power supply, it consumes just 13 mA. But then suddenly, it increased 94 mA. I measured resistance between GND and VDD_MCU pins. I was 53 ohm. I unders...

Makif by Associate
  • 1406 Views
  • 1 replies
  • 0 kudos

Resolved! stm32WB Security standar

Hi!I've some doubts about security features of stm32WB.After reading the documentation, forums, etc; I can find that stm32WB implements all 4 security levels of Security Mode 1, which includes the ECDHE P-256 cryptography.I've some questions about th...

j.villar by Associate II
  • 2017 Views
  • 1 replies
  • 1 kudos

Random BLE connection fail on STM32WB

Hello all,We are developing a product that connects to a mobile application through BLE. Sometimes, not all the time, the product does not connect to the smartphone the first time, it retries to connect until it gets there. As a consequence, the conn...

audrey38_0-1689064299779.png
audrey38 by Associate II
  • 1726 Views
  • 1 replies
  • 0 kudos

STM32WB55 Read Notify Characteristic Event

Hello,Is there any way to catch ACI event dedicated to read NOTIFY characteristic?I tought about ACI_ATT_READ_RESP_EVENT event, but I'm not sure if it is correct if I use with notify Characeristic.Could you confirm me that is a good way to achieve wh...

dnj by Associate III
  • 1392 Views
  • 1 replies
  • 0 kudos

Purchaing 'Qualification Fee' for using BlueNRG module

Hi  I am planning to use the BlueNrg module in my project , until I found out that I have to pay for the Qualification fee for using BlueTooth. Not sure if I dont display the logo I dont have to purchase it, or do I have to purchase it even if the lo...

Zigbee with standby mode

Hello,I have a board with stm32wb55 used as end device, I've tried to enter standby mode after connecting to zigbee network.I found out that if HSE is selected as RF wakeup clockPeriphClkInitStruct.RFWakeUpClockSelection = RCC_RFWKPCLKSOURCE_HSE_DIV1...

Corn Fan by Associate
  • 2997 Views
  • 2 replies
  • 0 kudos

What is the maximum value of HS_STARTUP_TIME for BlueNRG-1?

Hi friend,I want to extend the HS_STARTUP_TIME for BlueNRG-1. What is the maximum value of HS_STARTUP_TIME for BlueNRG-1? I saw the datasheet AN4494 it says that "XTAL_startup = XTAL_startup_measured*1.2*1.1*1.3 = 1.716*XTAL_startup_measured".  So 19...

TWu.6 by Associate II
  • 1105 Views
  • 1 replies
  • 0 kudos

ACI_GAP_SET_DISCOVERABLE adding TX power auto

Adding the TX power as standard on a GAP command.Is it part of some standard (SIG) of just an ST specific implementation? Also please refer to my ticket: https://community.st.com/t5/wireless-mcu/advertisement-start-without-automatically-adding-a-tx-p...

muslimah_0-1690369248717.png
muslimah by Associate II
  • 1654 Views
  • 1 replies
  • 1 kudos

STM32WB55 dual stack?

Good morning.I have an application where I want to have a Zigbee stack and a BLE stack both loaded on the STM32WB55.  Is this possible?  I would like my application firmware to be able to communicate with either stack exclusively depending on certain...

SWenn.1 by Senior III
  • 1052 Views
  • 1 replies
  • 0 kudos